JAJSBZ3B June 2014 – March 2018 LM46000
PRODUCTION DATA.
The LM46000 is internally compensated and the internal R-C values are 400 kΩ and 50 pF, respectively. Depending on the VOUT and frequency FS, if the output capacitor COUT is dominated by low ESR (ceramic types) capacitors, it could result in low phase margin. To improve the phase boost an external feed-forward capacitor CFF can be added in parallel with RFBT. Choose CFF so that phase margin is boosted at the crossover frequency without CFF. A simple estimation for the crossover frequency without CFF (fx) is shown in Equation 21, assuming COUT has very small ESR.
Equation 22 was tested for CFF:
Equation 22 indicates that the crossover frequency is geometrically centered on the zero and pole frequencies caused by the CFF capacitor.
For designs with higher ESR, CFF is not required when COUT has very high ESR and CFF calculated from Equation 22 should be reduced with medium ESR.Table 2 can be used as a quick starting point.
For the application in this design example, a 33-pF COG capacitor is selected.