JAJSF96C April 2018 – October 2021 LM5036
PRODUCTION DATA
The following schematic shows an example of an isolated half-bridge DC-DC converter controlled by LM5036 device. The operating input voltage range is 36-V to 75-V, and the output voltage is 12-V. The maximum load current is 8-A and the output current limit is configured to be 10-A.