JAJSF96C April 2018 – October 2021 LM5036
PRODUCTION DATA
A diode must be connected between the primary output VAUX1 and the VCC pin. When VAUX1 is more than one diode voltage drop greater than the internal VCC voltage, the VCC bias current is supplied from VAUX1. This results in reduced power losses in the internal VCC regulator, especially at high input voltage.