Careful PCB layout is critical to achieve low EMI and stable power supply operation as well as optimal efficiency. Make the high frequency current loops as small as possible, and follow these guidelines of good layout practices:
- For high power board design, use at least a
4-layer PCB of 2oz or thicker copper planes. Make the first inner layer a
ground plane that is adjacent to the top layer on which the power components
are installed, and use the second inner layer for the critical control
signals including the current sense, gate drive, commands, and so forth. The
ground plane between the signal and top layers helps shield switching noises
on the top layer away from affecting the control signals.
- Optimize the component placements and orientations before routing any traces. Place the power components such that the power flow from port to port is direct, straight and short. Avoid making the power flow path zigzag on the board.
- Identify the high frequency AC current loops. In
the bidirectional converter, the AC current loop of each channel is along
the path of the HV-port rail capacitors, high-side MOSFET, low-side MOSFET,
and back to the return of the HV-port rail capacitor. Place these components
such that the current flow path is short, direct and the special area
enclosed by the loop is minimized.
- Place the power circuit symmetrically between CH-1 and CH-2. Split the HV-port rail capacitors and LV-port rail capacitors evenly between CH-1 and CH-2.
- If more than one LM5171-Q1 is used on the same PCB for multi phases, place the
circuits of each LM5171-Q1 in the similar
pattern.
- Use adequate copper for the power circuit, so as
to minimize the conduction losses on high-current PCB tracks. Adequate
copper can also help dissipate the heat generated by the power components,
especially the power inductors, power MOSFETs, and current sense resistors.
However, pay attention to the polygon of the switch node, which connects the
high-side MOSFET source, low-side MOSFET drain, power inductor, and the
controller SW pin. The switch node polygon sees high dv/dt during switching
operation. To minimize the EMI emission by the switch node polygon, make its
size sufficient but not excessive to conduct the switched current.
- Use appropriate number of via holes to conduct current to, and heat through, the inner layers.
- Always separate the power ground from the analog ground, and make a single point connection of the power ground, analog ground, and the EP pad, at the location of the PGND pin.
- Minimize current-sensing errors by routing each pair of CSA and CSB traces using a kelvin-sensing directly across the current sense resistors. The pair of traces must be routed closely side by side for good noise immunity.
- Route sensitive analog signals of the CS, FBLV,
FBHV, IPK, VSET, IMON, COMP and OVP pins away from the high-speed switching
nodes (HB, HO, LO, and SW).
- Route the paired gate drive traces, namely the
pairs of HO1 and SW1, HO2 and SW2, LO1 and return, and LO2 and return,
closely side by side. Route CH-1 gate drive traces in symmetry with that of
CH-2.
- Place the device setting, programming and
controlling components as close as possible to the corresponding pins,
including the following component: ROSC, RCFG,
RDT, , CCOMP1, RCOMP2,
CCOMP1, CCOPM2, CHF1, CHF2,
RHVC, RLVC, CHVC, CLVC,
CHVHF and CLVHF.
- Place the bypass capacitors as close as possible
to the corresponding pins, including CHV, CVCC,
CVDD, CVREF, CVSET, CHB1,
CHB2, COVP, CIPK, CISET,
CCS1, CCS2 as well as the 100-pF current sense
common-mode bypassing capacitors.
- Flood each layer with copper to take up the empty areas for optimal thermal performance.
- Apply heat sink to components as necessary according to the system requirements.