JAJSRI9B October 2023 – June 2024 LM51772
PRODUCTION DATA
The integrated peak current sensor enables a low inductive sensing as it is located in series with the main inductor. It also can monitor the peak inductor current under all operation modes (boost, buck-boost and buck ) as well as for both current directions i.e. the bi-directional operation.
As the integrated sensor supports high bandwidth signals a differential mode filter adopted to the selected operating point is recommended for best performance. For most applications we recommend a resistor value for R(DIFF1/2) of 10 Ω. You can use the equation below to determine the filter capacitor:
Where the differential filter should be set to a 10th of the minimum on-time of Buck or Boost mode. See Figure 5-19 or Figure 5-21
Current sense resistors consist a parasitic inductance based on their geometry and the selected component vendors design. If the desired application requires high currents the impact of the external component parasitic can be reduced by placing multiple sense resistors in parallel.