JAJSRX5 November 2023 LM5185
PRODUCTION DATA
The LM5185 is a flyback DC/DC controller with integrated N-channel power MOSFET gate driver that can sink a peak current of 2 A and source a peak current of 1 A. During the MOSFET on-time, the transformer primary current increases from zero with a slope of VIN / LMAG (where LMAG is the transformer primary-referred magnetizing inductance) while the output capacitor supplies the load current. When the MOSFET is turned off by the gate driver, the switch voltage VSW swings up to approximately VIN + (NPS × VOUT), where NPS = NP/NS is the primary-to-secondary turns ratio of the transformer. The magnetizing current flows in the secondary side through the flyback diode, charging the output capacitor and supplying current to the load. Duty cycle D is defined as tON / tSW, where tON is the MOSFET conduction time and tSW is the switching period.
Figure 7-1 shows a typical schematic of the LM5185 PSR flyback circuit. Components denoted in red are optional depending on the application requirements.