JAJSP89 November 2024 LM5190
PRODUCTION DATA
In the voltage loop, the LM5190 has a high-gain transconductance amplifier that generates an error current proportional to the difference between the feedback voltage and an internal precision reference (0.8V). The transconductance of the amplifier is 1000µS. The voltage loop error amplifier only takes control when the internal minimum function block IMIN selector selects the current from the voltage loop error amplifier. See Section 6.3.14 for more details regarding the constant-current constant-voltage operation.
A type-II compensation network is generally recommended for peak current-mode control.