The LM61430-Q1 is designed to have very low input supply current when regulating
light loads. This is achieved by powering much of the internal circuitry from the
output. The BIAS pin is the input to the LDO that powers the majority of the control
circuits. By connecting the BIAS input pin to the output of the regulator, a small
amount of current drawn from the output. This current is reduced at the input by the
ratio of VOUT / VIN.
Equation 4. ![GUID-5B158449-3865-48BD-8EDF-542574ED1CDB-low.gif](/ods/images/JAJSKE1/GUID-5B158449-3865-48BD-8EDF-542574ED1CDB-low.gif)
where
- IQ_VIN(SW) = Current consumed by the
operating (switching) buck converter while
unloaded
- IQ_VIN = Nonswitching input current.
See IQ_VIN in the Electrical
Characteristics.
- IEN = Current drawn by the EN
terminal. Include this current if EN is connected
to VIN. See IEN in the Electrical
Characteristics. Note that this current
drops to a very low value if connected to a
voltage less than 5 V.
- Idiv = Current drawn by the feedback
voltage divider used to set output voltage
- ηeff Light-load efficiency of the buck
converter with IQ_VIN removed from the
input current of the buck converter.
ηeff = 0.8 is a conservative value that
can be used under normal operating
conditions.