As with any power conversion device, the LM614xxT-Q1 dissipates internal power while operating.
The effect of this power dissipation is to raise the internal temperature of the
converter above ambient temperature. The internal die temperature (TJ) is
a function of the following:
- Ambient temperature
- Power loss
- Effective thermal resistance,
RθJA of the device
- PCB layout
The maximum internal die temperature for the
LM614xxT-Q1 must be limited to 150°C. This limit establishes a limit on the
maximum device power dissipation and, therefore, the load current.
Equation 8 shows the relationships between the important parameters. Larger ambient
temperatures (T
A) and larger values of R
θJA reduce the maximum
available output current. The converter efficiency can be estimated by using the
curves provided in the
Application Curves section. If the desired operating conditions
cannot be found in one of the curves, then interpolation can be used to estimate the
efficiency. Alternatively, the EVM can be adjusted to match the desired application
requirements and the efficiency can be measured directly. The correct value of
R
θJA is more difficult to estimate. As stated in the
Semiconductor and IC Package Thermal Metrics application
note, the value of R
θJA given in the
Section 6.4 is not
valid for design purposes and must not be used to estimate the thermal performance
of the device in a real application. The values reported in the
Section 6.4 table
are measured under a specific set of conditions that are rarely obtained in an
actual application.
Equation 8.
where
- η = efficiency
- TA = ambient temperature in °C
- TJ = junction temperature in °C
- RθJA = the effective thermal
resistance of the IC junction to the air, mainly through the PCB in °C/W
The effective RθJA is a critical
parameter and depends on many factors (just to mention a few of the most critical
parameters:
- Power dissipation
- Air temperature
- Airflow
- PCB area
- Copper area
- Heatsink size
- Number of thermal vias under
or near the package
- Adjacent component
placement
Due to the ultra-miniature size of the VQFN (VAM) package, a die-attach pad is
not available, requiring most of the heat to flow from the pins to the board. This
action means that this package exhibits a somewhat large R
θJA value when
the layout does not allow for heat to flow from the pins. A typical curve of maximum
output current versus ambient temperature is shown in
Figure 8-2 for a good thermal layout. This data was taken on the LM61495TVAMEVM evaluation
board with a device and PCB combination, giving an R
θJA of about 21°C/W.
Remember that the data given in these graphs are for illustration purposes only, and
the actual performance in any given application depends on all of the previously
mentioned factors.
Use the following resources as a guide to
excellent thermal PCB design and estimating RθJA for a given application
environment: