JAJSJO5A October 2022 – October 2023 LM64460-Q1
PRODUCTION DATA
The purpose of spread spectrum is to eliminate peak emissions at specific frequencies by spreading these emissions across a wider range of frequencies. In most systems containing the LM64460-Q1, low-frequency conducted emissions from the first few harmonics of the switching frequency can be easily filtered. A more difficult design criterion is reduction of the emissions at higher harmonics that fall in the FM frequency band. These harmonics often couple to the environment through electric fields around the switch node and inductor. The LM64460-Q1 uses a ±2% spread of frequencies, which can spread energy smoothly across the FM and TV bands but is small enough to limit subharmonic emissions below the converter switching frequency. Peak emissions at the switching frequency of the converter are only reduced slightly, by less than 1 dB, while peaks in the FM band are typically reduced by more than 6 dB.
Use the MODE/SYNC pin to enable or disable spread spectrum in the LM64460-Q1. The LM64460-Q1 uses a cycle-to-cycle frequency hopping method based on a linear feedback shift register (LFSR). This intelligent pseudo-random generator limits cycle-to-cycle frequency changes to limit output ripple. The pseudo-random pattern repeats at less than 1.5 Hz, which is below the audio band.
Spread spectrum is only available while the clock of the LM64460-Q1 is free running at its natural frequency. Any of the following conditions overrides spread spectrum, turning it off: