SNOSDF8 December 2024 LM74680
PRODUCTION DATA
For the LM74680 to operate its top gates TG1 and TG2 in regulated conduction mode, the gate driver must be enabled as described in Section 7.3.3 and the current from source to drain of the external MOSFET must be within the range to result in an INx to OUTP voltage drop of VREV to VTG_FC. During forward regulation mode, the INx to OUTP voltage is regulated to VTG_REG by adjusting the gate to source voltage. This closed loop regulation scheme enables graceful turn-off of the MOSFET at very light loads and ensures zero DC reverse current flow.