JAJSF08G October 2017 – December 2020 LM74700-Q1
PRODMIX
PIN | I/O(1) | DESCRIPTION | |
---|---|---|---|
NO. | NAME | ||
1 | VCAP | O | Charge pump output. Connect to external charge pump capacitor |
2 | GND | G | Ground pin |
3 | EN | I | Enable pin. Can be connected to ANODE for always ON operation |
4 | CATHODE | I | Cathode of the diode. Connect to the drain of the external N-channel MOSFET |
5 | GATE | O | Gate drive output. Connect to gate of the external N-channel MOSFET |
6 | ANODE | I | Anode of the diode and input power. Connect to the source of the external N-channel MOSFET |
PIN | I/O(1) | DESCRIPTION | |
---|---|---|---|
NO. | NAME | ||
1 | EN | I | Enable pin. Can be connected to ANODE for always ON operation |
2 | GND | G | Ground pin |
3 | N.C | No connection | |
4 | VCAP | O | Charge pump output. Connect to external charge pump capacitor |
5 | ANODE | I | Anode of the diode and input power. Connect to the source of the external N-channel MOSFET |
6 | GATE | O | Gate drive output. Connect to gate of the external N-channel MOSFET |
7 | N.C | No connection | |
8 | CATHODE | I | Cathode of the diode. Connect to the drain of the external N-channel MOSFET |