JAJSOX6 October 2023 LM74930-Q1
PRODUCTION DATA
A minimum of 1-µF CVS capacitance is required. During input overvoltage transient, resistor RVS and Zener diode, DZ, are used to protect VS pin from exceeding the maximum ratings by clamping VVS to 60 V. Choosing RVS = 10 kΩ, the peak power dissipated in Zener diode DZ can be calculated using Equation 10 .
Where VDZ is the breakdown voltage of Zener diode. Select the Zener diode that can handle peak power requirement.
Peak power dissipated in resistor R1 can be calculated using Equation 11.
Select a resistor package which can handle peak power and maximum DC voltage.