JAJSIL9A February 2020 – July 2020 LM76005-Q1
PRODUCTION DATA
The LM76005-Q1 is designed to operate from an input voltage supply range between 3.5 V and 60 V. This input supply must be able to withstand the maximum input current and maintain a voltage above 3.5 V. The resistance of the input supply rail must be low enough that an input current transient does not cause a high enough drop at the LM76005-Q1 supply voltage that can cause a false UVLO fault triggering and system reset.
If the input supply is located more than a few inches from the LM76005-Q1, additional bulk capacitance can be required in addition to the ceramic bypass capacitors. The amount of bulk capacitance is not critical, but a 47-µF or 100-µF electrolytic capacitor is a typical choice.