JAJSRA4 September 2023 LMG3624
ADVANCE INFORMATION
The LMG3624 implements cycle-by-cycle overcurrent protection for the GaN power FETs. Figure 8-4 shows the cycle-by-cycle overcurrent operation. Every IN logic-high cycle turns on the GaN power FET. If the GaN power FET drain current exceeds the overcurrent threshold current, the overcurrent protection turns off the GaN power FET for the remainder of the IN logic-high duration.
An overcurrent protection event is not reported on the FLT pin. Cycle-by-cycle overcurrent protection minimizes system disruption because the event is not reported and because the protection allows the GaN power FET to turn on every IN cycle.
As described in the Current-Sense Emulation section, an artificial CS pin current is produced after the low-side GaN power FET is turned off by the low-side overcurrent protection, to prevent the controller from entering a hung state.