JAJSFX7E November 2004 – August 2018 LMH6574
PRODUCTION DATA.
The LMH6574 is optimized for maximum speed and performance in the small form factor of the standard SOIC package. To ensure maximum output drive and highest performance, thermal shutdown is not provided. Therefore, it is of utmost importance to make sure that the TJMAX is never exceeded due to the overall power dissipation.
Follow these steps to determine the Maximum power dissipation for the LMH6574:
where
where
The maximum power that the LMH6574 package can dissipate at a given temperature can be derived with the following equation:
where
For the SOIC package RθJA is 130 °C/W.