JAJSGV2D January 2012 – September 2021 LMK01801
PRODUCTION DATA
Sets the polarity of a SYNCX input pin. When SYNC is asserted the clock outputs will transition to a low state.
A pull-up on the SYNCX pin results in normal operation when the SYNCX_POL_INV = 1 and the SYNCX input is a no connect.
See Section 9.4.6 for more information on SYNC. A SYNC event can be generated by toggling this bit through the MICROWIRE interface.
R3[14, 15] | Polarity |
---|---|
0 | SYNC is active high |
1 | SYNC is active low |