JAJSGV2D January 2012 – September 2021 LMK01801
PRODUCTION DATA
When SYNC1_QUAL is set clock outputs on Bank B will be synchronized.
CLKout12 will be used as the SYNC qualification clock.
Only CLKout12 and CLKout13 support dynamic digital delay. However, this permits the relative phase relationship between CLKout12 and CLKout13 to be dynamically adjusted with respect to all other clock outputs. When NO_SYNC_CLKoutX_Y = 1, the corresponding clock outputs will not be interrupted during the SYNC event.
Qualifying the SYNC means that the pulse which turns the clock outputs off and on will have a fixed time relationship with the phase of the other clock outputs.
See Section 9.3.9 for more information.
R3[11] | Mode |
---|---|
0 (0x00) | No Qualification |
1 (0x01) | Reserved |
2 (0x10) | Reserved |
3 (0x11) | Qualification Enabled |