JAJSFA5E September 2015 – April 2018 LMK03318
PRODUCTION DATA.
The PLL has a Smart Input MUX. The input selection mode of the PLL can be configured using the 3-state REFSEL pin or programmed through I2C. The Smart Input MUX supports auto-switching and manual-switching using control pin (or through register). The Smart Input MUX is designed such that glitches created during switching in both auto and manual modes are suppressed at the MUX output.
In the automatic mode, the frequencies of both primary (PRIREF) and secondary (SECREF) input clocks have to be within 2000 ppm. The phase of the input clocks can be any. To minimize phase jump at the output, TI recommends setting very low PLL loop bandwidth, set R29.7 = 1 and R51.7 = 1; the outputs that are not muted should have its respective mute bypass bit in R20 and R21 be set to 0 to ensure that these outputs are available during an input switchover event. In the case that the primary reference is detected to be unavailable, the input MUX automatically switches from the primary reference to the secondary reference. When primary reference is detected to be available again, the input MUX switches back to the primary reference. When both primary and secondary references are detected as unavailable, the input MUX waits on secondary reference until either the primary or the secondary reference is detected as available again. When both the primary and secondary reference inputs are detected as unavailable, LOS is active, and the PLL outputs are automatically disabled. The timing diagram of an auto-switch at the input MUX is shown in Figure 43.
R50[1-0] are the register bits that control the smart input MUX for the PLL and can be programmed through I2C. Table 3 shows the input clock selection options for the PLL that are supported by the REFSEL pin or through I2C programming.
R50.1 | R50.0 | REFSEL | MODE | PLL REFERENCE |
---|---|---|---|---|
0 | 0 | X | Automatic | PLL prefers primary |
0 | 1 | 0 | Manual | PLL selects primary |
0 | 1 | VIM | Manual | PLL selects secondary |
0 | 1 | 1 | Automatic | PLL prefers primary |
1 | 0 | X | Manual | PLL selects primary |
1 | 1 | X | Manual | PLL selects secondary |
For those applications requiring device start-up from a crystal on the secondary input, do a one-time-only switchover to the primary input once available and, when auto-switch on the PLL's smart MUX is enabled, R51.2 can be set to 0 which automatically disables the secondary crystal input path after switchover to the primary input is complete. This removes coupling between the primary and secondary inputs and prevents input crosstalk components from appearing at the outputs. However, if the auto-switch between primary and secondary is desired at any point of normal device operation, R51.2 must be set to 1, PLL must be set to a very low loop bandwidth, and R20, R21, and R22 must be set to 0x0 to ensure minimal phase hit once PLL is relocked after switchover to either primary or secondary inputs. Figure 44 shows flowchart of events triggered when R51.2 is set to 1 or 0 .