10.5.6 Read SRAM
The contents of the SRAM can be read out, one word at a time, starting with that of the requested address. The following details the programming sequence for an SRAM read by address:
- Write the most significant 9th bit of the SRAM address in R139.0 and write the least significant 8 bits of the SRAM address in R140.
- The SRAM data located at the address specified in the step above can be obtained by reading R142 in the same I2C transaction. Any additional access that is part of the same transaction will cause the SRAM address to be incremented and a read will take place of the next SRAM address. Access to SRAM will terminate at the end of current I2C transaction.
NOTE
It is possible to increment SRAM address incorrectly when 2 successive accesses are made to R140.