JAJSDF8B March 2017 – July 2019 LMK04616
PRODUCTION DATA.
The LMK04616 features a total of 16 PLL2 clock outputs driven from one of the internal VCOs.
All PLL2 clock outputs have programmable output types. They can be programmed to HSDS or HCSL.
If OSCout is included in the total number of clock outputs the LMK04616 is able to distribute up to 17 differential clocks.
The following sections discuss specific features of the clock distribution channels that allow the user to control various aspects of the output clocks.