JAJSJN4C May 2020 – November 2022 LMK04832-SP
PRODUCTION DATA
When PLL1 is used, an external VCXO is required. The close-in noise performance of this VCXO is critcal for good jitter cleaning performance. The LMK04832-SP also provides OSCout, which by power-on default is a buffered copy of the PLL1 feedback and PLL2 reference input at OSCin. This reference input is typically a low noise VCXO or XO. This output can be used to clock external devices such as microcontrollers, FPGAs, CPLDs, and so forth, before the LMK04832-SP is programmed.