JAJSFI6C Februray 2017 – May 2018 LMK04832
PRODUCTION DATA.
Dynamic digital delay allows the phase of clocks to be changed with respect to each other with little impact to the clock signal.
For the device clock dividers this is accomplished by substituting the regular clock divider with an alternate divide value of one larger than the regular divider for one cycle. This substitution will occur a number of times equal to the value programmed into the DDLYd_STEP_CNT field for all outputs with DDLYdX_EN = 1.
For the SYSREF divider an alternate divide value will be substituted for the regular divide value. This substitution will occur a number of times equal to the value programmed into the DDLYd_STEP_CNT if DDLYd_SYSREF_EN = 1. To achieve one cycle delay as is done for the device clock dividers, set the SYSREF_DDLY value to one greater than SYSREF_DIV+SYSREF_DIV/2. For example, for a SYSREF divider of 100, to achieve 1 cycle delay, SYSREF_DIV = 100 + 50 + 1 = 151.
While using the Dynamic Digital Delay feature, CLKin_OVERRIDE must be set to 0.