SNOSB80C February 2011 – October 2015 LMP8350
PRODUCTION DATA.
While the main signal path frequencies may be fairly low, the ultra low distortion and settling time specifications rely on wide internal bandwidths. Precautions usually taken for high-speed amplifiers should be followed to maintain the best settling times and lowest distortion specifications. In order to get maximum benefit from the differential circuit architecture, board layout and component selection is very critical. The circuit board should have low a inductance ground plane and well bypassed broad supply lines. External components should be leadless surface mount types. The feedback network and output matching resistors should be composed of short traces and precision resistors (0.1%). The output matching resistors should be placed within 3-4 mm of the amplifier as should the supply bypass capacitors.
The LMP8350 is sensitive to parasitic capacitances on the outputs. Ground and power plane metal should be removed from beneath the amplifier and from beneath RF and RG.
With any differential signal path symmetry is very important. Even small amounts of asymmetry will contribute to distortion and balance errors. Special attention should be paid to where the bypass capacitors are grounded, as this also affects settling and distortion performance.
The LMH730154 evaluation board is an example of good layout techniques. Evaluation boards are available for purchase through the product folder on TI’s website.
The LMP8350 is optimized for maximum performance in the small form factor of the standard SOIC package, and is essentially a dual-channel amplifier. To ensure maximum output drive and highest performance, thermal shutdown is not provided. Therefore, it is of utmost importance to make sure that the TJMAX of 150°C is never exceeded due to the overall power dissipation.
Follow these steps to determine the Maximum power dissipation for the LMP8350:
where
where
The maximum power that the LMP8350 package can dissipate at a given temperature can be derived from Equation 7:
where
NOTE
If VOCM is not 0 V then there will be quiescent current flowing in the feedback network. This current should be included in the thermal calculations and added into the quiescent power dissipation of the amplifier.
Generally, a good high-frequency layout will keep power supply and ground traces away from the inverting input and output pins. Parasitic capacitances on these nodes to ground will cause frequency response peaking and possible circuit oscillations (see Application Note OA-15 (SNOA367) for more information). Texas Instruments suggests the following evaluation boards in Table 4 as a guide for high-frequency layout and as an aid in device testing and characterization:
DEVICE | PACKAGE | EVALUATION BOARD PART NUMBER | ||
---|---|---|---|---|
LMP8350MA | SOIC | LMH730154 |