JAJSPU7 June 2024 LMR36503E-Q1
PRODUCTION DATA
In some cases, an input UVLO level different than that provided internal to the device is needed. This need can be accomplished by using the circuit shown in Figure 8-2. The input voltage at which the device turns on is designated as VON while the turnoff voltage is VOFF. First, a value for RENB is chosen in the range of 10kΩ to 100kΩ, then Equation 11 and Equation 12 are used to calculate RENT and VOFF respectively.
where