JAJSR13 December 2024 LMR60420
PRODMIX
Minimum on-time refers to the minmum amount of time the high side MOSFET can turn on. The LMR60420 regulates the output voltage even if the input-to-output voltage ratio requires an on-time less than the minimum on-time, tON-MIN, for the given frequency setting. The LMR60420 accomplishes this by folding back the switching frequency to support the same input-to-output voltage ratio while maintaining an on-time of tON-MIN. The LMR60420 can support a minimum on-time of 30ns (typical). Equation 7 can be used to estimate the on-time for a given operating condition.
Where: