SNAS879 December 2024 LMR60420
PRODMIX
The LMR60420 is a step-down DC–DC converter, typically used to convert a higher DC voltage to a lower DC voltage with a maximum output current of 2A. The following design procedure can be used to select components for the LMR60420. Refer to the following figure for a reference schematic as well as the following table to assist in component selection.