JAJSR66 September 2024 LMR66430-EP
PRODUCTION DATA
The LMR66430-EP dissipates internal power while operating. The effect of this power dissipation is to raise the internal temperature of the converter above ambient. The internal die temperature (TJ) is a function of the ambient temperature, the power loss, and the effective thermal resistance, RθJA, of the device, and PCB combination. The maximum junction temperature for the LMR66430-EP must be limited to 150°C. This limit establishes a limit on the maximum device power dissipation and, therefore, the load current. Equation 12 shows the relationships between the important parameters. See that larger ambient temperatures (TA) and larger values of RθJA reduce the maximum available output current.
The converter efficiency can be estimated by using the curves provided in this data sheet. If the desired operating conditions cannot be found in one of the curves, interpolation can be used to estimate the efficiency. Alternatively, the EVM can be adjusted to match the desired application requirements and the efficiency can be measured directly. The correct value of RθJA is more difficult to estimate. For more information, refer to the Semiconductor and IC Package Thermal Metrics application report.
This design case temperature is measured in Figure 8-12. The temperature gradient between top case and junction is often only a few degrees (celsius), so this measurement can determine the thermal margin on a given design
where
The effective RθJA is a critical parameter and depends on many factors such as the following:
The IC junction temperature can be estimated for a given operating condition using Equation 13.
where
The IC power loss mentioned above is the overall power loss minus the loss that comes from the inductor DC resistance.
The following figure is provided to estimate the thermal resistance of the IC for a particular board area.
Use the following resources as guides to optimal thermal PCB design and estimating RθJA for a given application environment: