JAJSSL5 December 2023 LMX1906-SP
PRODUCTION DATA
Use the clock multiplier to multiply up the input clock frequency by a factor of x2, x3, or x4. The multiply value is set by the CLK_MULT field. As the multiplier is PLL-based and includes an integrated VCO, the multiplier has a state machine clock, requires calibration, has a lock detect feature. Note that if the multiplier is not used, there is no need for the state machine clock or the lock detect feature.