12.1.1 Configuring the LMX2541 for Optimal Performance
Determine the Channel Spacing (fCH)
For a system that has a VCO that tunes over several frequencies, the channel spacing is the tuning increment. In the case that the VCO frequency is fixed, this channel spacing is the greatest number that divides both the VCO frequency and the OSCin frequency.
Determine OSCin Frequency (fOSCin)
If the OSCin frequency is not already determined, then there are several considerations. A higher frequency is generally, but not always, preferable. One reason for this is that it has a higher slew rate if it is a sine wave. Another reason is that the clock for the VCO frequency calibration is based on the OSCin frequency and in general will run faster for higher OSCin frequencies.
Although a higher OSCin frequency is desirable, there are also reasons to use a lower frequency. If the OSCin frequency is strategically chosen, the worst case fractional spur channels might fall out of band. Also, if the OSCin frequency can be chosen such that the fractional denominator can avoid factors of 2 and/or 3, the sub-fractional spurs can be reduced.
Determine the Phase Detector Frequency (fPD) , Charge Pump Gain (KPD) and Fractional Denominator (FDEN)
In general, choose the highest phase detector frequency and charge pump gain, unless it leads to loop filter capacitor values that are unrealistically large for a given loop bandwidth. In this case, reducing either the phase detector frequency or the charge pump gain can yield more feasible capacitor values. Other reasons for not using the highest charge pump gain is to allow some adjustment margin to compensate for changes in the VCO gain or allow the use of Fastlock.
For choosing the fractional denominator, start with FDEN = fPD/fCH. As discussed previously, there might be reasons to choose larger equivalent fractions.
Design the Loop Filter
Determine the Modulator Order
Determine Dithering and Potential Larger Equivalent Fractional Value