When the device is first powered up, it must to be initialized, and the ordering of this programming is important. The sequence is listed below. After this sequence is completed, the device should be running and locked to the proper frequency.
- Apply power to the device and ensure the Vcc pins are at the proper levels.
- If CE is LOW, pull it HIGH.
- Wait 100 µs for the internal LDOs to become stable.
- Ensure that a valid reference is applied to the OSCin pin.
- Program register R0 with RESET=1. This will ensure all the registers are reset to their default values.
- Program in sequence registers R60, R58, R53, …, R1 and then R0.