JAJSFI5 May 2018 LMX2572LP
PRODUCTION DATA.
First, determine all the elementary blocks of a synthesizer.
Then, program these registers to make LMX2572LP locks to the target output frequency:
Then program these registers to enable FSK SPI FAST mode:
A Mathlab script is then developed to generate the necessary codes that will be used to continuously bit-stream the LMX2572LP. These codes are uploaded to the data generator DG2020, which will generate the SPI data to modulate the LMX2572LP.