JAJSEF4P April 2012 – January 2024 LP5907
PRODUCTION DATA
The LP5907 can be switched on or off by a logic input at the EN pin. A voltage on this pin greater than VIH turns the device on, and a voltage less than VIL turns the device off.
When the EN pin is low, the regulator output is off and the device typically consumes less than 1μA. Additionally, an output pulldown circuit is activated that makes sure any charge stored on COUT is discharged to ground.
If the application does not require the shutdown feature, the EN pin can be tied directly to the IN pin to keep the regulator output permanently on.
An internal 1MΩ pulldown resistor ties the EN input to ground, making sure the device remains off if the EN pin is left open circuit. To provide proper operation, the signal source used to drive the EN pin must be able to swing above and below the specified turn-on or turn-off voltage thresholds listed in the Electrical Characteristics under VIL and VIH.