SNVS469F October 2006 – December 2015 LP5952
PRODUCTION DATA.
For availability of evaluation boards, refer to the product folder of LP5952 at www.ti.com.
For information regarding evaluation boards, please refer to AN-1531 LP5952 Evaluation Board (SNVA188).
The following links connect to TI community resources. Linked contents are provided "AS IS" by the respective contributors. They do not constitute TI specifications and do not necessarily reflect TI's views; see TI's Terms of Use.
E2E is a trademark of Texas Instruments.
All other trademarks are the property of their respective owners.
These devices have limited built-in ESD protection. The leads should be shorted together or the device placed in conductive foam during storage or handling to prevent electrostatic damage to the MOS gates.
SLYZ022 — TI Glossary.
This glossary lists and explains terms, acronyms, and definitions.