JAJSSO2 December 2023 MCF8315C
PRODMIX
The DC bus current limit feature can be used to limit the current supplied by the DC input source (VM). This feature can be enabled by setting BUS_CURRENT_LIMIT_ENABLE to 1b. The DC bus current limit can be configured using BUS_CURRENT_LIMIT. This feature limits the DC bus current by limiting the speed (SPEED_REF_LIM)/current (CURRENT_REF_LIM) reference as shown in Figure 6-48. Enabling this feature may restrict the speed/phase current of the motor from reaching the set point (SPEED_REF or CURRENT_REF) in order to limit the DC bus current. The DC bus current limit status is reported on BUS_CURRENT_LIMIT_STATUS.