SLLSFX9 December 2024 MCF8316D
PRODUCTION DATA
The input reference can be a speed, power, current or voltage command as configured by INPUT_REFERENCE_MODE.
Speed Reference Transfer Function
Figure 6-23 shows the relationship between DUTY_CMD and SPEED_REF. MAX_SPEED sets the SPEED_REF at DUTY_CMD of 100%. MIN_DUTY sets the minimum SPEED_REF (MIN_DUTY x MAX_SPEED). If MAX_SPEED is set to 0-Hz, SPEED_REF is clamped to zero (irrespective of DUTY_CMD) and motor is in stopped state.
Power Reference Transfer Function
Figure 6-24 shows the relationship between DUTY_CMD and POWER_REF. MAX_POWER sets the POWER_REF at DUTY_CMD of 100%. MIN_DUTY sets the minimum POWER_REF (MIN_DUTY x MAX_POWER). If MAX_POWER is set to 0-W, POWER_REF is clamped to zero (irrespective of DUTY_CMD) and motor is in stopped state.
Voltage Reference Transfer Function
In voltage reference mode, the phase voltage applied to motor is proportional to the DUTY_CMD (from MIN_DUTY to 100%) as shown in Figure 6-25. For DUTY_CMD less than MIN_DUTY, the applied voltage to motor is clamped to zero.
Current Input Transfer Function
Figure 6-26 shows the relationship between DUTY_CMD and CURRENT_REF. ILIMIT sets the CURRENT_REF at DUTY_CMD of 100%. MIN_DUTY sets the minimum CURRENT_REF (MIN_DUTY x ILIMIT).