JAJSUY7 May 2024 MCT8316A-Q1
PRODUCTION DATA
High-side braking mode is configured by setting MTR_STOP to 011b. When a motor stop command is received, the output speed is reduced to a value defined by ACT_SPIN_BRK_THR prior to turning all high-side MOSFETs ON (see example Figure 6-43) for a time configured by MTR_STOP_BRK_TIME. If the motor speed is below ACT_SPIN_BRK_THR prior to receiving stop command, then the MCT8316A-Q1 transitions directly into the brake state. After applying the brake for MTR_STOP_BRK_TIME, the MCT8316A-Q1 transitions into Hi-Z state by turning OFF all MOSFETs.