JAJSDQ7C June 2017 – September 2018 MSP430FR6035 , MSP430FR6037 , MSP430FR60371 , MSP430FR6045 , MSP430FR6047 , MSP430FR60471
PRODUCTION DATA.
Figure 5-6 shows the average LPM currents vs wake-up frequency at 25°C.
NOTE:
The average wake-up current does not include the energy required in active mode; for example, for an interrupt service routine or to reconfigure the device.Figure 5-7 shows the average LPM currents vs wake-up frequency at 85°C.
NOTE:
The average wake-up current does not include the energy required in active mode; for example, for an interrupt service routine or to reconfigure the device.