JAJSKN5B April 2021 – December 2021 OPA3S2859-EP
PRODUCTION DATA
デバイスごとのパッケージ図は、PDF版データシートをご参照ください。
By using the latch control input for each channel, the feedback selection can be controlled separately from the common SEL1 and SEL0 pins, see an example below. The latch control inputs can also provide benefits in some cases where channel A and B need to have the same configuration. For example, in transparent mode, when switching between different gain settings any timing skew from SEL1 and SEL0 may result in unintended switch logic configurations for a short-duration resulting in transient output glitch. These intermediate glitch states can be minimized by holding the LTCH_x pin low until the new selection value at SEL pins has settled.
This feature is also useful in larger systems with multiple OPA3S2859-EP devices, the gain path can be set using common SEL0 and SEL1 signals for all the devices and latch pins can be used to control the gain independently for each amplifier channel.
Example configuration, to update the gain settings for Channel A only, follow these steps:
1. Set LTCH_B to logic low (latch mode), this way changes made on Channel A do not affect Channel B gain configuration.
2. If LTCH_A is high (transparent mode), use SEL0 and SEL1 pins to select the feedback network of interest. If LTCH_A is low, toggle it to logic high and use SEL0 and SEL1 pins to select the feedback network of interest.
3. To hold the selected gain, set LTCH_A to logic low. Ensure minimum setup time requirements (100 ns) are met between SELx selection to LTCH_A going low. Also, ensure that during the hold time (100 ns), no changes should be made on SELx pins. The minimum timing is based on internal device configuration, if needed, additional time must be added due to board layout parasitics and signal delays.
4. Gain setting for channel A is now latched and any changes on SELx pins will not change the gain configuration for channel A.