JAJSNK9A December 2021 – December 2022 OPT4001
PRODUCTION DATA
CRC register consists of Cyclic Redundancy Checker bits part of the output registers calculated within the OPT4001 device and updated on every measurement. This feature helps in detecting communication related bit errors during the output readout from the device. The calculation method for the CRC bits is shown in Figure 8-14, which can be independently verified in the controller or host firmware/software to validate if communication between the controller and the device was successful without bit errors during transmission.