JAJSVR9K December 2005 – December 2024 PCA9557
PRODUCTION DATA
Data is transmitted to the PCA9557 by sending the device address and setting the least-significant bit (LSB) to a logic 0 (see Figure 7-7 for device address). The command byte is sent after the address and determines which register receives the data that follows the command byte. There is no limitation on the number of data bytes sent in one write transmission (see Figure 7-9 and Figure 7-10).