SBAS448B October 2008 – August 2015 PCM1690
PRODUCTION DATA.
デバイスごとのパッケージ図は、PDF版データシートをご参照ください。
For the PMC1690 application support, see the following:
For related documentation, see the following:
Dynamic Performance Testing of Digital Audio D/A Converters, SBAA055
The following links connect to TI community resources. Linked contents are provided "AS IS" by the respective contributors. They do not constitute TI specifications and do not necessarily reflect TI's views; see TI's Terms of Use.
E2E is a trademark of Texas Instruments.
Blu-ray is a trademark of Blu-ray Disk Association.
I2S is a trademark of NXP Semiconductors.
All other trademarks are the property of their respective owners.
These devices have limited built-in ESD protection. The leads should be shorted together or the device placed in conductive foam during storage or handling to prevent electrostatic damage to the MOS gates.
SLYZ022 — TI Glossary.
This glossary lists and explains terms, acronyms, and definitions.