JAJSKU0A December 2020 – June 2021 PCM1820 , PCM1821
PRODUCTION DATA
The device record channel includes a high dynamic range, built-in digital decimation filter to process the oversampled data from the multibit delta-sigma (ΔΣ) modulator to generate digital data at the same Nyquist sampling rate as the FSYNC rate. The decimation filter can be chosen from two different types only in slave mode, depending on the required frequency response, group delay, and phase linearity requirements for the target application. The selection of the decimation filter option can be done by the MD0 pin. Table 8-7 shows the decimation filter mode selection for the record channel.
MD0 | DECIMATION FILTER MODE SELECTION (Supported Only in Slave Mode) |
---|---|
LOW | Linear phase filters are used for the decimation in slave mode. For master mode, the device always use linear phase filters for the decimation. |
HIGH | Low latency filters are used for the decimation in slave mode. For master mode, the device always use linear phase filters for the decimation. |