JAJSUM7 May 2024 PCM1841-Q1
ADVANCE INFORMATION
The device consists of four pairs of analog input pins (INxP and INxM) as differential inputs for the recording channel. The device supports simultaneous recording of up to four channels using the high-performance multichannel ADC. The input source for the analog pins can be from the electret condenser analog microphones, micro electrical-mechanical system (MEMS) analog microphones, or line-in (auxiliary) inputs from the system board.
The voice or audio signal inputs must be capacitively coupled (AC-coupled) to the device. For better distortion performance, use the low-voltage coefficient capacitors for AC coupling. The device has the typical input impedance on INxP or INxM as 2.5kΩ on each pin. The value of the coupling capacitor in AC-coupled mode must be chosen so that the high-pass filter formed by the coupling capacitor and the input impedance do not affect the signal content. Before proper recording can begin, this coupling capacitor must be charged up to the common-mode voltage at power-up. The device has a quick charge scheme that increases the charging speed of the coupling capacitor at power-up. The default value of the quick-charge timing is set for a coupling capacitor up to 1µF.