SLLSEO3 July 2015 SN65HVD63
PRODUCTION DATA.
Control Interface for Antenna Line Devices, Antenna Interface Standards Group, Standard No. AISG v2.0
The following links connect to TI community resources. Linked contents are provided "AS IS" by the respective contributors. They do not constitute TI specifications and do not necessarily reflect TI's views; see TI's Terms of Use.
E2E is a trademark of Texas Instruments.
AISG is a registered trademark of Antenna Interface Standards Group, Ltd.
All other trademarks are the property of their respective owners.
These devices have limited built-in ESD protection. The leads should be shorted together or the device placed in conductive foam during storage or handling to prevent electrostatic damage to the MOS gates.
SLYZ022 — TI Glossary.
This glossary lists and explains terms, acronyms, and definitions.