JAJSF06A March 2018 – May 2018 SN65LVDS93B
PRODUCTION DATA.
The SN65LVDS93B does not require a specific power-up sequence.
The device is permitted to power up IOVCC while VCC, VCCPLL, and VCCLVDS remain powered down and connected to GND. The input level of the SHTDN during this time does not matter as only the input stage is powered up while all other device blocks are still powered down.
The device is also permitted to power up all 3.3-V power domains while IOVCC is still powered down to GND. The device will not suffer damage. However, in this case, all the I/Os are detected as logic HIGH, regardless of their true input voltage level. Hence, connecting SHTDN to GND will still be interpreted as a logic HIGH; the LVDS output stage turns on. The power consumption in this condition is significantly higher than standby mode, but still lower than normal mode.
The user experience can be impacted by the way a system powers up and powers down an LCD screen. The following sequence is recommended:
Power-up sequence (SN65LVDS93B SHTDN input initially low):
Power-down sequence (SN65LVDS93B SHTDN input initially high):