JAJSIP3 February 2020 SN74HCS21-Q1
PRODUCTION DATA.
In this application, one channel of the SN74HCS21-Q1 is used as shown in Figure 9. The additional channel can be used individually or the inputs can be grounded and the channel left unused.
The SN74HCS21-Q1 is used to drive the RESET pin of the system controller. When any of the inputs to the gates become LOW, the controller will be disabled. The controller will only operate when all inputs are HIGH, indicating normal operation.