SCES581D JULY 2004 – October 2015 SN74LVC1GX04
UNLESS OTHERWISE NOTED, this document contains PRODUCTION DATA.
デバイスごとのパッケージ図は、PDF版データシートをご参照ください。
NOTE
Information in the following applications sections is not part of the TI component specification, and TI does not warrant its accuracy or completeness. TI’s customers are responsible for determining suitability of components for their purposes. Customers should validate and test their design implementation to confirm system functionality.
The SN74LVC1GX04 contains a buffered and unbuffered inverter for the specific purpose of creating a crystal oscillator and driver with limited external components.
Figure 5 shows a typical application of the SN74LVC1GX04 in a Pierce oscillator circuit. The buffered inverter (SN74LVC1G04 portion) produces a rail-to-rail voltage waveform. The recommended load for the crystal shown in this example is 16 pF. The value of the recommended load (CL) can be found in the crystal manufacturer's data sheet.
Values of C1 and C2 are chosen to calculate CL in Equation 1 where C1 ≡ C2.
Rs is the current-limiting resistor, and the value depends on the maximum power dissipation of the crystal. Generally, the recommended value of Rs is specified in the crystal manufacturer's data sheet and, usually, this value is approximately equal to the reactance of C2 at resonance frequency, that is seen in Equation 2.
RF is the feedback resistor that is used to bias the inverter in the linear region of operation. Usually, the value is chosen to be within 1 MΩ to 10 MΩ.
The open-loop gain of the unbuffered inverter decreases as power-supply voltage decreases. This decreases the closed-loop gain of the oscillator circuit. The value of Rs can be decreased to increase the closed-loop gain, while maintaining the power dissipation of the crystal within the maximum limit.
Rs and C2 form a low-pass filter and reduce spurious oscillations. Component values can be adjusted, based on the desired cutoff frequency.
C2 can be increased over C1 to increase the phase shift and help in start-up of the oscillator. Increasing C2 may affect the duty cycle of the output voltage.
At high frequency, phase shift due to Rs becomes significant. In this case, Rs can be replaced by a capacitor to reduce the phase shift.
After the selection of proper component values, the oscillator circuit should be tested using these components. To ensure that the oscillator circuit performs within the Recommended Operating Conditions, follow these steps: