JAJSKB1N December 2003 – June 2024 SN74LVC1T45
PRODUCTION DATA
To begin the design process, determine the following:
• Input voltage range
- Use the supply voltage of the device that is driving the SN74LVC1T45 device to determine the input voltage range. For a valid logic high the value must exceed the VIH of the input port. For a valid logic low the value must be less than the VIL of the input port.
• Output voltage range
- Use the supply voltage of the device that the SN74LVC1T45 device is driving to determine the output voltage range.