Add a decoupling capacitor from VCC to
GND. The capacitor needs to be placed physically close to
the device and electrically close to both the VCC
and GND pins. An example layout is shown in the Layout
Example section.
Ensure the capacitive load at the output is ≤ 70pF. This is not a hard limit; by design, however,
it will optimize performance. This can be
accomplished by providing short, appropriately
sized traces from the SN74LVC3G57 to the receiving device.
Ensure the resistive load at the output is larger
than (VCC / IO(max)) Ω, so that the
maximum output current from the Absolute Maximum
Ratings is not violated. Most CMOS inputs have a
resistive load measured in mega ohms; much larger than the
minimum calculated previously.
Thermal issues are rarely a concern for logic
gates, however the power consumption and thermal increase can be calculated
using the steps provided in the application report, CMOS Power
Consumption and Cpd Calculation